MPC5775 SPT FFT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5775 SPT FFT

2,783 Views
ronliu
Contributor IV

HI all,

I'd like to use the SPT module. We can see that there is a FFT core in the SPT. But what should I do to make it work ? Is there some code sample to share? Thanks

Regards,

Ron

 

155286_155286.png7.png

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

2,231 Views
jinjingyang
NXP Employee
NXP Employee

The attachment is the example project in GHS for MPC5775K. It demonstrate how to use SPT to do a 256 FFT.

Maybe you already got that. It's the only example code for FFT at this moment.

0 Kudos
Reply

2,231 Views
martin_kovar
NXP Employee
NXP Employee

Hi Ron,

unfortunately, we do not have any example, how to use FFT core. I also had asked our application engineer about some app notes or documents, but I got the answer there no such documents.

This module is too complex to create some simple example. Solutions are created exactly for user application. You can order professional support service, which helps you to create the application. Please look at the following URL:

Professional Support for Microcontrollers|NXP

Regards,

Martin

0 Kudos
Reply

2,231 Views
ronliu
Contributor IV

Martin,

Thanks a lot. I'll try to contact the support.

Regards,

Ron

0 Kudos
Reply