MPC574xG AUTOSAR OS problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC574xG AUTOSAR OS problem

Jump to solution
10,253 Views
Ehsaaan
Contributor III

Hello,

I am working on the MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3 sample from NXP. When I open sample_sc1 in EB Tresos V14.2 and try to generate it, I faced two errors. 
I attached the error log from EB. 

 

Regards,

Ehsan

0 Kudos
Reply
1 Solution
10,217 Views
namnguyenviet
NXP Employee
NXP Employee

Then you need to check the java RTE version: it should be 6.0 or higher, and it must be a 32-bit version. Here is mine:

namnguyenviet_0-1634719510142.png

 

View solution in original post

7 Replies
10,228 Views
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

You may try to:

- Goto the folder "..\NXP\AUTOSAR\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\os_ts\eclipse\workspace\os_sample_sc1\output\epc>

- Then call "...\NXP\AUTOSAR\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\ssc\bin\generator\sg.exe project.epc"

- Then check if the configuration is generated successfully in the "...\NXP\AUTOSAR\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\os_ts\eclipse\workspace\os_sample_sc1\output"

 

Best regards,

Hung

0 Kudos
Reply
10,226 Views
Ehsaaan
Contributor III

Hello

I did that and this is the result, please take a look:
and there is just a project.epc file in the output folder.

Regards,
Ehsan

0 Kudos
Reply
10,218 Views
namnguyenviet
NXP Employee
NXP Employee

Then you need to check the java RTE version: it should be 6.0 or higher, and it must be a 32-bit version. Here is mine:

namnguyenviet_0-1634719510142.png

 

8,090 Views
spara7c5
Contributor III

Hello Namn,
i get the same error on the external generator.
My java setup is:

spara7c5_0-1709668647668.png


Can you help?

0 Kudos
Reply
10,206 Views
Ehsaaan
Contributor III

Its ok now. the problem was JAVA version. Thanks.

Regards,
Ehsan

0 Kudos
Reply
10,234 Views
namnguyenviet
NXP Employee
NXP Employee
0 Kudos
Reply
10,225 Views
Ehsaaan
Contributor III

Thanks, it was useful, But it didn't help.

Regards,
Ehsan

0 Kudos
Reply