MPC574xG AUTOSAR OS problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC574xG AUTOSAR OS problem

跳至解决方案
10,272 次查看
Ehsaaan
Contributor III

Hello,

I am working on the MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3 sample from NXP. When I open sample_sc1 in EB Tresos V14.2 and try to generate it, I faced two errors. 
I attached the error log from EB. 

 

Regards,

Ehsan

0 项奖励
回复
1 解答
10,236 次查看
namnguyenviet
NXP Employee
NXP Employee

Then you need to check the java RTE version: it should be 6.0 or higher, and it must be a 32-bit version. Here is mine:

namnguyenviet_0-1634719510142.png

 

在原帖中查看解决方案

7 回复数
10,247 次查看
hungnguyenphi
NXP Employee
NXP Employee

Hello @Ehsaaan ,

 

You may try to:

- Goto the folder "..\NXP\AUTOSAR\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\os_ts\eclipse\workspace\os_sample_sc1\output\epc>

- Then call "...\NXP\AUTOSAR\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\ssc\bin\generator\sg.exe project.epc"

- Then check if the configuration is generated successfully in the "...\NXP\AUTOSAR\MPC574xG_AUTOSAR_OS_4_0_92_RTM_1_0_3\os_ts\eclipse\workspace\os_sample_sc1\output"

 

Best regards,

Hung

0 项奖励
回复
10,245 次查看
Ehsaaan
Contributor III

Hello

I did that and this is the result, please take a look:
and there is just a project.epc file in the output folder.

Regards,
Ehsan

0 项奖励
回复
10,237 次查看
namnguyenviet
NXP Employee
NXP Employee

Then you need to check the java RTE version: it should be 6.0 or higher, and it must be a 32-bit version. Here is mine:

namnguyenviet_0-1634719510142.png

 

8,109 次查看
spara7c5
Contributor III

Hello Namn,
i get the same error on the external generator.
My java setup is:

spara7c5_0-1709668647668.png


Can you help?

0 项奖励
回复
10,225 次查看
Ehsaaan
Contributor III

Its ok now. the problem was JAVA version. Thanks.

Regards,
Ehsan

0 项奖励
回复
10,253 次查看
namnguyenviet
NXP Employee
NXP Employee
0 项奖励
回复
10,244 次查看
Ehsaaan
Contributor III

Thanks, it was useful, But it didn't help.

Regards,
Ehsan

0 项奖励
回复