MPC5748G windiss simulator - GDB-server???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G windiss simulator - GDB-server???

1,030件の閲覧回数
rami_rosenbaum
Contributor II

Hi,

I'm working on the NXP MPC5748G board and want to develop on the windiss simulator as well.

Does it have a GDB-server? Very little info on the net...

This is how I'm running windiss:

PS C:\> windiss -tPPC C:\WindRiver\diab\5.9.4.8\example\powerpc\bubble.out
Initial array: 10 9 8 7 6 5 4 3 2 1
Number of tests: 90
Sorted array:  1 2 3 4 5 6 7 8 9 10
windiss: Task finished, exit code: 0, Instructions executed: 19378
windiss: Interrupts were never enabled

Thanks.

タグ(3)
0 件の賞賛
返信
0 返答(返信)