MPC5748G USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G USB

Jump to solution
4,831 Views
tony_huang
Contributor III

Hi,

      We now using MPC5748G USB Host and OTG module, and I  cannot find any demos in the MPC5 software example list. So I just  wondering if there is something that we can get start from, rather than getting start from nothing.

0 Kudos
Reply
1 Solution
4,503 Views
tony_huang
Contributor III

Hi,

      Is there MPC5748G USB  example right now. You said that USB  example would  be released in July 2017.

View solution in original post

6 Replies
3,906 Views
chenwilsoft
Contributor III

I have installed the last version of SDK for MPC5748G (3.0.3). There are 2 USB demos in the SDK. But the USB of MPC5748G acts HOST in these demos. Is there any example of the USB which works as SLAVE in OTG mode?

0 Kudos
Reply
4,503 Views
tony_huang
Contributor III

Thans a lot!

0 Kudos
Reply
4,503 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, we do not have any USB example right now, but there will be a driver for USB as a part of MPC5748G SDK, which will be released in July 2017.

Regards,

Martin

0 Kudos
Reply
4,504 Views
tony_huang
Contributor III

Hi,

      Is there MPC5748G USB  example right now. You said that USB  example would  be released in July 2017.

4,503 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

The information I have is that USB should be a part of MPC5748G SDK which will be release on 27th July.

Regards,

Martin

0 Kudos
Reply
4,503 Views
tony_huang
Contributor III

Hi,

 Is  MPC5748G USB  example released  today, and  how can I  get the demo?

 Regards,

 Tom_Chen

0 Kudos
Reply