MPC5748G PWM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G PWM

3,057件の閲覧回数
sohyunjang
Contributor III

Hi, I use MPC5748G PWM.

I have referred to the Cookbook below.
And I changed the PWM channel.
PG[2] ->PE[13]

void emios1_ch23_MCB(void) {    /* Config emios 1 chan 23: MCB, 1K count */

  eMIOS_UC_1.UC[23].C.R = 0x0; /* Disable channel prescaler (reset default) */
  eMIOS_UC_1.UC[23].A.R = 1000; /* MCB mode: period will be 1K clocks */
  eMIOS_UC_1.UC[23].C.B.MODE = 0x50; /* Modulus Counter Buffered (Up ctr) */
  eMIOS_UC_1.UC[23].C.B.UCPRE = 0; /* Prescale channel clock by 0+1=1 */
  eMIOS_UC_1.UC[23].C.B.UCPREN= 1; /* Enable prescaler */
}

void emios1_ch11_OPWMB(void) {      /* Config emios 1 chan 1: OPWMB */

  eMIOS_UC_1.UC[20].C.R = 0x0; /* Disable channel prescaler (reset default) */
  eMIOS_UC_1.UC[20].A.R = 250; /* PWM leading edge count value */
  eMIOS_UC_1.UC[20].B.R = 500; /* PWM trailing edge count value */
  eMIOS_UC_1.UC[20].C.B.BSL = 0; /* Timebase: counter bus A (chan 23) */
  eMIOS_UC_1.UC[20].C.B.EDPOL = 1; /* Output polarity on A match */
  eMIOS_UC_1.UC[20].C.B.MODE = 0x60; /* Output Pulse Width Modulation Buf'd*/
  SIUL2.MSCR[77].B.SSS = 1; /* Pad PG2: Source signal is E1UC_11_H */
  SIUL2.MSCR[77].B.OBE = 1; /* Pad PG2: OBE=1 (LED1 on Freescale EVB) */
}

There is no PWM output from PE13.
I changed it to PE12 and confirmed the PWM output was normal.

Is that a problem?
ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,907件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

set SIUL2.MSCR[77].B.SSS = 2;

BR, Petr

0 件の賞賛
返信

2,775件の閲覧回数
syerlank
Contributor I

@PetrS  Hello,

I'm using PF[6] for eMIOS_0_23_X and PP[13] for eMIOS_1_23_X. I'm able to get PWM output for PF[6] (eMIOS_0_23_X) but I'm not able to see PWM output for PP[13] (eMIOS_1_23_X). I also enabled global prescaled clock and time base for both emios0 and 1. Below is code snippet, can you please assist me? 

/*-------eMIOS_0_23_X ----------*/

eMIOS_UC_0.UC[23].C.R = 0x0;
eMIOS_UC_0.UC[23].A.R = 20;
eMIOS_UC_0.UC[23].B.R = 200;
eMIOS_UC_0.UC[23].CNT.R = 1;
eMIOS_UC_0.UC[23].C.B.EDPOL = 1; 
eMIOS_UC_0.UC[23].C.B.MODE = 0x58;
eMIOS_UC_0.UC[23].C.B.UCPRE = 0;
eMIOS_UC_0.UC[23].C.B.UCPREN= 1;

SIUL2.MSCR[86].B.SSS = 1;
SIUL2.MSCR[86].B.OBE = 1;
SIUL2.MSCR[86].B.src=3 or 4;

/*-------eMIOS_0_23_X ----------*/

 

/*-------eMIOS_1_23_X ----------*/

eMIOS_UC_1.UC[23].C.R = 0x0; 
eMIOS_UC_1.UC[23].A.R = 20; 
eMIOS_UC_1.UC[23].B.R = 200;
eMIOS_UC_1.UC[23].CNT.R = 1;
eMIOS_UC_1.UC[23].C.B.EDPOL = 1;
eMIOS_UC_1.UC[23].C.B.MODE = 0x58; 
eMIOS_UC_1.UC[23].C.B.UCPRE = 0; 
eMIOS_UC_1.UC[23].C.B.UCPREN= 1;

SIUL2.MSCR[253].B.SSS = 1; 
SIUL2.MSCR[253].B.OBE = 1; 
SIUL2.MSCR[253].B.src=3; 

/*-------eMIOS_1_23_X ----------*/

 

0 件の賞賛
返信