MPC5748G - IC5500 Flash Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G - IC5500 Flash Issue

3,023件の閲覧回数
stso
Contributor III

Hello,

 

I wanted to switch from the PE Micro Universal FX Debugger to the ISystem IC5500. I tried to flash the elf-files I received by  compiling an empty S32-Design Studio project created by the wizard.

When starting to download the files I get the following error:

 

Error in download(): E_FAIL: isystem.connect call failed. / Error 22: Can not start emulation. Check Vcc and clock source

The connection with the debugger was tested and is working properly. Vcc is at 12 V. The steps I took are the same as described here:

winIDEA Help 

(except that I tried to use JTAG to flash and I choose the IC5500).

 

 Regards,

Stefan

ラベル(1)
0 件の賞賛
返信
1 返信

2,736件の閲覧回数
stso
Contributor III

I figured it out. When I left work yesterday a colleague of mine wanted to have a closer look at the EVB, pulled off the daughtercard and didn't put it back on properly.

0 件の賞賛
返信