MPC5748G - How to reduce startup time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G - How to reduce startup time?

2,406 Views
xierxiaofeng
Contributor II

Hello, 

      I am using MCP5748G. It takes about more than 100ms to work properly after powering up.  How many milliseconds is the normal startup time? How to reduce startup time?

Thanks!

0 Kudos
Reply
6 Replies

2,388 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Startup of device is defined in the datasheet:

petervlna_0-1737013356590.png

This is time when voltage is applied to the point where is device released from reset and can start executing code.

If you are referring to SW startup time, then this will of course vary on how good/optimized is your code written and what it all does and will vary on each customer application requirements.

In general, if you write it in ASM it will save you a lot of time.

Best regards,

Peter

 

0 Kudos
Reply

2,300 Views
xierxiaofeng
Contributor II
Hi Peter,
Thanks your reply. I measured the clock initialization time with an oscilloscope to be about 130ms, is this time normal? How to shorten the clock initialization time.

Best regards
0 Kudos
Reply

2,268 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I measured the clock initialization time with an oscilloscope to be about 130ms, is this time normal?

Well, since you are using some drivers which are based on platform and not optimized specially for this device, the time can be various. there will be huge overhead compared to ASM init code.

in reality, to setup clocks in shortest possible time would require approximately 100 instructions.

Please always refer to your driver documentation for execution time.

NXP usually release those in quality package of drivers.

It will also depends on how do you measure the execution time. Measuring with some driver toggling pin will be much different from tracing the instruction execution with advanced debuggers.

best regards,

Peter

0 Kudos
Reply

2,258 Views
xierxiaofeng
Contributor II
Hi Peter,
Thanks your replay.
Where to find driver doucment for execution time?Could you please provide ASM init code?

best regards,
xierxiaofeng
0 Kudos
Reply

2,213 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Where to find driver doucment for execution time?

Driver documentation is usually accompanied with driver. NXP has it either directly in the driver doc folder or in the quality package which is located at NXP SW account along with driver installation.

petervlna_1-1739433206285.png

 

Could you please provide ASM init code?

No. The point to write ASM code is to have it optimized for your application.

best regards,

Peter

 

0 Kudos
Reply

2,298 Views
xierxiaofeng
Contributor II

Init System ClcokInit System Clcok图片.png图片.png

The execution time of three lines of code is about 130ms

 

0 Kudos
Reply