[MPC5748G] CAN FD Multiple Instances

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MPC5748G] CAN FD Multiple Instances

ソリューションへジャンプ
3,488件の閲覧回数
BenMW
Contributor I

Hi, for my project I want to use all of the 8 Flexcan Modules. When I use the first instance like in the example project, the physical bus works fine with interrupt/error handling. 

During initialization I can see that the ESR1 registers of CAN1...7 are not changing any values. CAN0 instance is set to SYNC and IDLE.

The initialization of every instance is performed by the FLEXCAN_DRV_Init() function:

/* Initialize FlexCAN driver */
FLEXCAN_DRV_Init(INST_FLEXCAN1, &flexcan1_State, &flexcan1_InitConfig0);
FLEXCAN_DRV_Init(INST_FLEXCAN2, &flexcan2_State, &flexcan2_InitConfig0);
FLEXCAN_DRV_Init(INST_FLEXCAN3, &flexcan3_State, &flexcan3_InitConfig0);
FLEXCAN_DRV_Init(INST_FLEXCAN4, &flexcan4_State, &flexcan4_InitConfig0);
FLEXCAN_DRV_Init(INST_FLEXCAN5, &flexcan5_State, &flexcan5_InitConfig0);
FLEXCAN_DRV_Init(INST_FLEXCAN6, &flexcan6_State, &flexcan6_InitConfig0);
FLEXCAN_DRV_Init(INST_FLEXCAN7, &flexcan7_State, &flexcan7_InitConfig0);
FLEXCAN_DRV_Init(INST_FLEXCAN8, &flexcan8_State, &flexcan8_InitConfig0); 

The structures for init are the same and they're generated by Processor Expert. After FLEXCAN_Enable(base) is called, ESR1 of CAN0 looks like the following:

BenMW_0-1629804174229.pngBenMW_0-1629804174229.png

On the other instances it looks different:

BenMW_1-1629804316672.pngBenMW_1-1629804316672.png

Does anyone knows why CAN1...7 are not enabled correctly? The MCR registers of the modules are the same:

BenMW_2-1629804576283.pngBenMW_2-1629804576283.png

 

BenMW_3-1629804603586.pngBenMW_3-1629804603586.png

Thanks a lot!

0 件の賞賛
返信
1 解決策
3,479件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

to be able to send anything, module must be synchronized to the bus and see it as idle, that is RDX pin must be high. Also module must see own transmitted signal. Transceiver ensures this.
For simple test without transceiver you can do external loopback connection, TXD to RXD. This way you can test proper pin initialization.

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,486件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

do you have pins configured as well in the pin_mux component for other CAN modules?
Moreover CAN modules must be connected with CAN transceivers.

BR, Petr 

0 件の賞賛
返信
3,481件の閲覧回数
BenMW
Contributor I

I know that I need transceivers for every CAN, but is it neccessary for initialization? In the first step I want to try error handling if transmitting a CAN frame is not possible. But because of the problem during initialization there is no interrupt generated (e.g. NACK).

0 件の賞賛
返信
3,480件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

to be able to send anything, module must be synchronized to the bus and see it as idle, that is RDX pin must be high. Also module must see own transmitted signal. Transceiver ensures this.
For simple test without transceiver you can do external loopback connection, TXD to RXD. This way you can test proper pin initialization.

BR, Petr

0 件の賞賛
返信
3,477件の閲覧回数
BenMW
Contributor I

Thanks for this information, it solves my problem!

It works if you just configure the pins for transceiver in the pinMux peripheral. No physical transceiver needed to check just error interrupt handling.

0 件の賞賛
返信