MPC5748G Bootloader boot application Failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G Bootloader boot application Failed

1,045件の閲覧回数
KangSong
Contributor I

Hi.

Sorry, my English is poor.

I got a bootloader and  a application, then i want to jump from bootlader to application。

when the bootloader is an empty project, I can use " (*(void (*)(void)) (0x01200000))();" to jump to the application. but when I added some functions to the bootloader, this method failed, Add I tried use " __asm__(" e_lis %r3, 0x0120");
__asm__(" e_ori %r3,%r3,0x0000");
__asm__(" se_mtlr %r3");
__asm__(" se_blr");", But this did not solve my problem。

And I confirmed that i did not erase the flash of the Application flash space when flashing the bootloader.

Why it does not work? How can i do this?

Here is detail configuration of my environment:

My Bootloader:

Bootloader FLASH_BASE_ADDR is 0x01000000;
Bootloader FLASH_SIZE is 2048K;

MEMORY
{
flash_rchw : org = 0x00F90000, len = 0x4
cpu0_reset_vec : org = 0x00F90000+0x10, len = 0x4
cpu1_reset_vec : org = 0x00F90000+0x14, len = 0x4
cpu2_reset_vec : org = 0x00F90000+0x04, len = 0x4
rappid_boot_data : org = 0x00F90000+0x08, len = 0x8

m_text : org = FLASH_BASE_ADDR, len = FLASH_SIZE
m_data : org = SRAM_BASE_ADDR, len = SRAM_SIZE
}

My Application:

/* Define FLASH */
/* FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x01000000; */
/* FLASH_SIZE = DEFINED(__flash_size__) ? __flash_size__ : 1856K; */
FLASH_BASE_ADDR = 0x01200000;
FLASH_SIZE = 2048K;

/* Define SRAM */
SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40000000;
SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 256K;

/* Define RAppID boot data address */
RAPPID_BOOT_APP_DELAY_ADDR = 0x00F9C008;
RAPPID_BOOT_APP_KEY_ADDR = 0x00F9C00C;

MEMORY
{
flash_rchw : org = 0x00F9C000, len = 0x4
cpu0_reset_vec : org = 0x00F9C000+0x10, len = 0x4
cpu1_reset_vec : org = 0x00F9C000+0x14, len = 0x4
cpu2_reset_vec : org = 0x00F9C000+0x04, len = 0x4
rappid_boot_data : org = 0x00F9C000+0x08, len = 0x8

m_text : org = FLASH_BASE_ADDR, len = FLASH_SIZE
m_data : org = SRAM_BASE_ADDR, len = SRAM_SIZE
}

Thanks in advance.

0 件の賞賛
返信
1 返信

1,033件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's highly recommended to put everything back to default reset state before jumping to user application. This is the most common reason.

There are two options:

- you can jump to the application right after reset

- or configure all used registers back to default state. The most important thing is to disable interrupts on all levels: by MSR[EE] bit in the core(s), by priorities in interrupt controller and by local enable bits in peripherals.

Regards,

Lukas

0 件の賞賛
返信