MPC5748G BAF usage (LIN0)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G BAF usage (LIN0)

1,254 Views
aurelienturban
Contributor I

Hello,

I am trying to developp BAF (Boot Assist Flash) programming for factory programming of our gateway.

At the moment I am using MPC5748G LCEVB.

I have experience with previous BAM , over can bus.This is my first BAF attempt.

In case of MPC5748G it seems BAF only works with serial communication over PB0 / PB1.

I connected my FTDI_RX to PB0_LIN0TX and FTDI_TX to PB1_LIN0RX.

Whole PFLASH is erased. ( FF value as seen on debugger ) so there is no valid boot header anywhere.

BAF area is programmed ( content that was delivered with the board ), attached.

As LCEVB xtal is 40 mhz, I have set up the baudrate to 48 000 baud as indicated in the reference manual, 8 data bit, no parity bit, 1 stop bit.

I am sending \h(FE ED FA CE CA FE BE) over FTDI , I checked on the logic analyser : the message is sent at 48 000 baud.

No response is received.

Any help appreciated.

Kind regards

0 Kudos
Reply
0 Replies