MPC5746c lower power

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746c lower power

1,470 Views
flight
Contributor II

How to minimize power consumption when entering STANDBY mode?What operations are required?

0 Kudos
Reply
1 Reply

1,368 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

You have to disable all power domains except PD0 (which is always active)

You have to run from IRC clock (SIRC or FIRC)

In this mode, the power supply is turned off for most of the chip. The only parts of the chip that are still powered during this mode are pads mapped on wakeup lines and power domain #0 which contains the MC_RGM, MC_PCU, WKPU etc.. The IRC can be optionally switched off. This is the lowest power consumption mode possible on the chip.

For the start you can refer to reference example code:

https://community.nxp.com/docs/DOC-343775 

regards,

Peter

0 Kudos
Reply