MPC5746R BD Hardware Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5746R BD Hardware Issue

1,067件の閲覧回数
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

 

Customer use MPC5746R BD (MAPBGA-292 package), and find the code can be downloaded but the external oscillator is not work.
Compare the H/W with the EVB schematic, the different is the voltage of VDD_HV_FLA, it's 5V not 3.3V.
Any suggestion is appreciate.

 

Best regards,

ラベル(1)
0 件の賞賛
返信
1 返信

971件の閲覧回数
hongpingxu-b364
NXP Employee
NXP Employee

Problem solved!

Customer forget to supply VDD_HV_IO_JTAG.

0 件の賞賛
返信