MPC5746C Clock Monitor Unit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C Clock Monitor Unit

1,952 Views
cholland
Contributor V

Hi,

I tried following the example here Using the CMU on the MPC5744 for IRCOSC Measurement and reading Application Note AN12080.

I seem to be getting different readings for each different Measurement Duration.

//---------------------------------------------------
F_CLKMN0_RMT (FXOSC) = 40 MHz
CMU.MDR.B.MD: 0x000FFFFF 1048575

CLKMT0_RMN (FIRC) (IRCOSC)
fd: 0x81BD6 531414
f_sel: 78927168.000000

CLKMT1 (SIRC)
fd: 0xFB2FA 1028858
f_sel: 40766560.000000

CLKMT2 (SXOSC)
fd: 0x7DA59 514649
f_sel: 81498264.000000

//---------------------------------------------------
F_CLKMN0_RMT (FXOSC) = 40 MHz
CMU.MDR.B.MD: 0x0001FFFF 131071

CLKMT0_RMN (FIRC) (IRCOSC)
fd: 0x5039F 328607
f_sel: 15954742.000000

CLKMT1 (SIRC)
fd: 0xA9831 694321
f_sel: 7551031.500000

CLKMT2 (SXOSC)
fd: 0x8F701 587521
f_sel: 8923664.000000

//---------------------------------------------------
F_CLKMN0_RMT (FXOSC) = 40 MHz
CMU.MDR.B.MD: 0x0000FFFF 65535

CLKMT0_RMN (FIRC) (IRCOSC)
fd: 0x281E4 164324
f_sel: 15952630.000000

CLKMT1 (SIRC)
fd: 0x4F55C 324956
f_sel: 8066938.500000

CLKMT2 (SXOSC)
fd: 0x4792A 293162
f_sel: 8941814.000000

void CMU_test(void)
{
float f_sel, diff;
unsigned long MD = 0xFFFF; //(0..1048575)

//---------------------------------------------------------------------------
// CLKMT0_RMN
//---------------------------------------------------------------------------

//1. Program the CMU_MDR[MD] (Measure Duration) value.
// (20 bits = 2^20 - 1 = 1048576 - 1 = 1048575)
CMU.MDR.B.MD = MD;

//2. Program the CMU_CSR[CKSEL1] bit to the CLKMT0_RMN you wish to measure.
CMU.CSR.B.CKSEL1 = CLKMT0_RMN;

//3. Enable the monitor by setting the CMU_CSR[SFM] bit.
CMU.CSR.B.SFM = 1;

//4. When the CMU_CSR[SMF] bit is clear read the CMD_FDR[FD] value and calculate the IRCOSC frequency.
while(CMU.CSR.B.SFM){}

f_sel = (float)F_CLKMN0_RMT * ((float)CMU.MDR.B.MD / (float)CMU.FDR.B.FD);


//---------------------------------------------------------------------------
// CLKMT1
//---------------------------------------------------------------------------
//1. Program the CMU_MDR[MD] value.
// (20 bits = 2^20 - 1 = 1048576 - 1 = 1048575)
CMU.MDR.B.MD = MD;

//2. Program the CMU_CSR[CKSEL1] bit to the CLKMT0_RMN you wish to measure.
CMU.CSR.B.CKSEL1 = CLKMT1;

//3. Enable the monitor by setting the CMU_CSR[SFM] bit.
CMU.CSR.B.SFM = 1;

//4. When the CMU_CSR[SMF] bit is clear read the CMD_FDR[FD] value and calculate the IRCOSC frequency.
while(CMU.CSR.B.SFM){}

f_sel = (float)F_CLKMN0_RMT * ((float)CMU.MDR.B.MD / (float)CMU.FDR.B.FD);

//---------------------------------------------------------------------------
// CLKMT2
//---------------------------------------------------------------------------
//1. Program the CMU_MDR[MD] value.
// (20 bits = 2^20 - 1 = 1048576 - 1 = 1048575)
CMU.MDR.B.MD = MD;

//2. Program the CMU_CSR[CKSEL1] bit to the CLKMT0_RMN you wish to measure.
CMU.CSR.B.CKSEL1 = CLKMT2;

//3. Enable the monitor by setting the CMU_CSR[SFM] bit.
CMU.CSR.B.SFM = 1;

//4. When the CMU_CSR[SMF] bit is clear read the CMD_FDR[FD] value and calculate the IRCOSC frequency.
while(CMU.CSR.B.SFM){}

f_sel = (float)F_CLKMN0_RMT * ((float)CMU.MDR.B.MD / (float)CMU.FDR.B.FD);

}

Thanks,

Labels (1)
1 Reply

1,665 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you should use proper MD value to ensure the FD does not overflow as there is no internal status of the FD overflow.

Thus the theoretical max MD value for each measured clock can be (assuming 40MHz reference clock)

- FIRC: maxMD = 16MHz/40MHz*1048575 = 419430

- SIRC: maxMD = 128KHz/40MHz*1048575 = 3355

- SXOSC: maxMD = 32KHz/40MHz*1048575 = 834

Use even smaller value to have some boundary if clock is not accurate.

BR, Petr