MPC5744p ethernet sample code and app note

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744p ethernet sample code and app note

2,848 Views
kitchix
Contributor I

I am currently investigating the ethernet driver on the MPC5744P. We have selected the 257 MBGA chip so the hardware should have all preconditions for it to work. I would like to have an application note and some sample code for the ethernet driver if you have that available, to start with.I have searched through this community site without any success yet.

Best regards

Martin

Labels (1)
0 Kudos
Reply
3 Replies

2,733 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Martin,

you can find the drivers and SW examples included in S32 Design Studio IDE:

S32 Design Studio IDE for Power Architecture based MCUs | NXP 

There's either simple ENET driver:

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.0\examples\MPC5744P\driver_examples\communication\enet_loopback\

or lwip stack:

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.0\examples\MPC5744P\demo_apps\lwip\

The documentation is included too. More information about lwip stack can be found here:

lwIP - A Lightweight TCP/IP stack - Summary [Savannah] 

lwIP Wiki | Fandom 

Regards,

Lukas

0 Kudos
Reply

2,731 Views
kitchix
Contributor I

Hi Lukas,

I don’t have the S32DS installed, have been looking for that to, but could not find it except to the update variants ? How can I get hold of a S32DS installation package ? It would be easier, if I did not need to use the S32DS environment, I already have plenty of development IDE’s. If you could just send med the code that you referes to ?

Best regards

/Martin

Skickades från E-post<https://go.microsoft.com/fwlink/?LinkId=550986> för Windows 10

Från: lukaszadrapa<mailto:[email protected]>

Skickat: den 27 april 2020 11:17

Till: Martin Karlsson<mailto:[email protected]>

Ämne: Re: - Re: MPC5744p ethernet sample code and app note

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: MPC5744p ethernet sample code and app note

reply from Lukas Zadrapa<https://community.nxp.com/people/lukaszadrapa?et=watches.email.thread> in MPC5xxx - View the full discussion<https://community.nxp.com/message/1303924?commentID=1303924&et=watches.email.thread#comment-1303924>

Hi Martin,

you can find the drivers and SW examples included in S32 Design Studio IDE:

S32 Design Studio IDE for Power Architecture based MCUs | NXP<https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.nxp.com%2Fdesign%2Fsoftware%2Fdevelopment-software%2Fs32-design-studio-ide%2Fs32-design-studio-for-power-architecture%3AS32DS-PA>

There's either simple ENET driver:

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.0\examples\MPC5744P\driver_examples\communication\enet_loopback\

or lwip stack:

c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.0\examples\MPC5744P\demo_apps\lwip\

The documentation is included too. More information about lwip stack can be found here:

lwIP - A Lightweight TCP/IP stack - Summary <https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsavannah.nongnu.org%2Fprojects%2Flwip%2F>

lwIP Wiki | Fandom<https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Flwip.fandom.com%2Fwiki%2FLwIP_Wiki>

Regards,

Lukas

Reply to this message by replying to this email, or go to the message on NXP Community<https://community.nxp.com/message/1303924?commentID=1303924&et=watches.email.thread#comment-1303924>

Start a new discussion in MPC5xxx by email<mailto:[email protected]> or at NXP Community<https://community.nxp.com/choose-container.jspa?contentType=1&containerType=14&container=11363&et=watches.email.thread>

Following Re: MPC5744p ethernet sample code and app note<https://community.nxp.com/message/1303924?commentID=1303924&et=watches.email.thread#comment-1303924> in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe<https://community.nxp.com/unsubscribe.jspa?email=martin.karlsson%40cpacsystems.se&token=eddf2672250c8784d83e39de14ef9353ed290dbd673d276d8c6594a02dd27e2f> instantly from NXP Community, or adjust email frequency in your email preferences<https://community.nxp.com/user-preferences!input.jspa>

0 Kudos
Reply

2,731 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Martin,

we do not provide these drivers in standalone form. An option is to extract the drivers from SDK but you would lose main advantage of the Processor Expert - graphical user interface for configuration. Unfortunately we can't help with this.

Regards,

Lukas

0 Kudos
Reply