MPC5744P

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P

1,701件の閲覧回数
amchengfeng
Contributor I

I purchased a SPC5744PFMLQ9 (PIN-144), powered up after soldering, and found that its reset pin (PIN31) is always low, even if it is connected to a 5K pull-up resistor, it is still low. After connecting with the JTAG debugger, it will report an error when debugging, as shown below.531.png

According to the S32DS prompt, I checked the reference manual, but I am not sure if the chip is locked. If it is locked, how should I unlock it?

pastedImage_3.png
I hope someone can help me, thanks.

0 件の賞賛
返信
1 返信

1,583件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

your problem is not related to locked microcontroller. If reset line is always 0, this means, microcontroller is still in reset and this could be caused by many reasons.

I suppose you have your own board design (please write me if I am wrong). First of all, I recommend you to check all hints from MPC5744P hardware design guide, please see the link below.

https://www.nxp.com/docs/en/application-note/AN5267.pdf 

Especially, be sure your power supply design is correct.

Regards,

Martin

0 件の賞賛
返信