MPC5744P efsdiv instruction compile error by Windriver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P efsdiv instruction compile error by Windriver

1,285 次查看
feiteng
Contributor I

I am using MPC5744P for a project.

I have set target option: -tPPCE200Z4251N3VEF:simple for compiler&assembler&linker of Windriver.

That is because I want to use EFPU (Embedded floating-point unit) to speed up the calculation.

However, when I was compiling X.c which have floating-point divide calculation, there always have compile error.

The compile error is as follow:
"XXX\llopt unrecognize line: efsdiv ?a8, ?a7, ?a6" . It seems like assembler can't recognize efsdiv instruction, but, it's unreasonable.

Actually, "efsdiv" instruction has been written in "E200Z4 reference manual".


PS:
1. The core of MPC5744P is E200Z4251N3;
2."llopt" is an executive program file of Windriver which is using for optimizing assembly file.

0 项奖励
回复
0 回复数