MPC5744P RTM SMCAL ISO26262 module defects update

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P RTM SMCAL ISO26262 module defects update

799 次查看
AndrewwDabach
Contributor II

Hi,

I could see that the last version of ISO26262 autosar SMCAL package for MPC5744P was version 2.0.2 in Dec 2018. (kindly correct me if I am wrong)

2.0.2 SW574XP-SMCL401-RTMC_SR-2.0.2Dec 5, 2018

 

But additionally there is also, this 'List of Known Defects' excel file, where the known defects in SMCAL are updated every week and in that, it was also mentioned next to those entered new defects that it is fixed too.

 MPC574xP SMCAL 4.0 'List Of Known Defects' weekly report
Report is updated weekly for active product only.
Dec 30, 2011

 

Now, I am confused that, whether the fixes of new weekly defects are updated regularly in the same v2.0.2 SMCAL link above or published somewhere else? Could you help me out?

Thanks and Regards

(https://nxp.flexnetoperations.com/control/frse/product?child_plneID=710837)

标记 (2)
0 项奖励
回复
1 回复

764 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have gone trough the weekly defects excel and compared it to the latest release.

Now, I am confused that, whether the fixes of new weekly defects are updated regularly in the same v2.0.2 SMCAL link above or published somewhere else? Could you help me out?

No, they are updated only in the case of release of new version of SW. I can see that last time we released:

MPC574XP MCAL4.0 swv: 2.0.2 RTM_HF1

Where I see last change in the weekly defects in December 2021. Since then there was no change in the release.

So if you stick with latest SW version it will match the weekly defect reports (which is just automatically generated from system).

Best regards,

Peter

 

0 项奖励
回复