MPC5744P Port Configure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P Port Configure

5,249 次查看
fyw
Contributor IV

145727_145727.pngpastedImage_0.png

This is MPC5744P A[0] Configure. I wander  if set like this:

MSCR[0].sss = 0001b

IMCR[48].sss = 0001b

IMCR[59].sss = 0010b

What will A[0] be?   Is there priority between MSCR[0].sss & IMCR[x].sss ? 

If I want to set IMCR[x].sss(for example like REQ0) , should I have to set MSCR[0].sss=0?

 

Thank you very much!

标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

4,296 次查看
fyw
Contributor IV

If I want use port A[0] as "etimer_0 input data channel 0", Which to choose?

A: MSCR[0].sss = 0001b

B: IMCR[59].sss = 0010b

C: both of A&B

D: ethier of A&B

Thank you!

0 项奖励
回复

4,296 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) MSCR[0].ibe = 1 to enable input buffer (sss field is not important when output functionality is disabled).

2) IMCR[59].sss = 0010b to route etimer_0 inpu_data_channel_0 to A[0] input buffer.

4,296 次查看
jaureshsieh
Contributor II

if i want to set A[0] to output pin.

A[0]MSCR[0]=0x0;

IMCR[xx]=xx?

how to set it?

0 项奖励
回复

4,296 次查看
alexvinchev
Contributor V

Sorry, syntax highlight here is awful...

You can use these macros to help you:

/* GPIO & SIUL macros */

#define PortOffset(pn)  (16 * pn)

#define Port(name,pin)  ((Port##name) + pin)

#define SIUL_Out(pin,sss) { \

SIUL2.MSCR[Port pin].B.SSS = sss; /* Pin functionality */ \

SIUL2.MSCR[Port pin].B.src=3; /* Maximum slew rate */ \

SIUL2.MSCR[Port pin].B.OBE = 1; /* Output Buffer Enable on */ \

SIUL2.MSCR[Port pin].B.IBE = 0; /* Input Buffer Enable off */ \

}

#define SIUL_In(pin,imcr,sss) { \

SIUL2.IMCR[imcr - 512].B.SSS = sss; /* Pin functionality */ \

SIUL2.MSCR[Port pin].B.OBE = 0; /* Output Buffer Enable off */ \

SIUL2.MSCR[Port pin].B.IBE = 1; /* Input Buffer Enable on */ \

}

/* Set value of GPIO output */

#define GPIO_VO(pin) SIUL2.GPDO[Port pin].B.PDO_4n

/* Get value of GPIO input */

#define GPIO_VI(pin) SIUL2.GPDI[Port pin].B.PDI_4n

/* Setup GPIO as output */

#define GPIO_Out(pin,v) { \

SIUL2.GPDO[Port pin].B.PDO_4n = v; /* Set initial pin value */ \

SIUL_Out(pin,0); /* Pin functionality as GPIO*/ \

}

/* Setup GPIO as input */

#define GPIO_In(pin) { \

SIUL2.MSCR[Port pin].B.SSS = 0; /* Pin functionality as GPIO*/ \

SIUL2.MSCR[Port pin].B.OBE = 0; /* Output Buffer Enable off */ \

SIUL2.MSCR[Port pin].B.IBE = 1; /* Input Buffer Enable on */ \

}

/* Usage example */

#define LED1GIO         (A,0)

#define LED1            GPIO_VO(LED1GIO)

void func(void){

    /* GPIO as output, initialized as 0 */

    GPIO_Out(LED1GIO, 0);

    /* Set value of GPIO to 1 */

    LED1 = 1;

}

0 项奖励
回复

4,296 次查看
alexvinchev
Contributor V
#define SIUL_Out(pin,sss) {                                                                 \
                        SIUL2.MSCR[Port pin].B.SSS = sss;   /* Pin functionality    */  \
                        SIUL2.MSCR[Port pin].B.src=3; /* Maximum slew rate    */  \
                        SIUL2.MSCR[Port pin].B.OBE = 1; /* Output Buffer Enable on  */  \
                        SIUL2.MSCR[Port pin].B.IBE = 0; /* Input Buffer Enable off  */  \
                    }

/* Setup GPIO as output */

#define GPIO_Out(pin,v) {                                                                       \

                            SIUL2.GPDO[Port pin].B.PDO_4n = v;  /* Set initial pin value    */  \

                            SIUL_Out(pin,0);                    /* Pin functionality as GPIO*/  \

                        }

0 项奖励
回复

4,296 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

IMCR register says how to route signal from particular input buffer to particular module (thus it is input configuration).

MSCR configures pad in general and selects its output configuration (SSS field says which particular module’s output signal is routed to the output buffer).

4,296 次查看
fyw
Contributor IV

Thank you very much! 

0 项奖励
回复