MPC5744P PMC test

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5744P PMC test

1,083 次查看
ismael-wael
Contributor II

Hello,

I am trying to test the PMC by applying fault injection using PMC_FIR register.

ismaelwael_0-1732009344792.png

here it says the MC_RGM should reset the MCU in case of fault injection, of course after proper setting of relevant registers. but that never happened whatever i do!

 

I thought maybe PMC needs to activate the clock, so i added these two lines:

/* Initialize clock gate*/
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);

 

still nothing.

I finally debugged the PMC registers, and found that whatever i write, i could not read it back as in code below:

int main(void)
{
  /* Write your local variable definition here */
  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
  #ifdef PEX_RTOS_INIT
    PEX_RTOS_INIT();                   /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of Processor Expert internal initialization.                    ***/
    /* Initialize clock gate*/
    CLOCK_SYS_Init(g_clockManConfigsArr,   CLOCK_MANAGER_CONFIG_CNT,
                   g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
    CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
  /* Initialize Pins */
  PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
 
 
  //PINS_DRV_ClearPins(PORT, (1<<LED)); // Led ON
  //PINS_DRV_SetPins(PORT, (1<<LED)); // Led Off
  //PMC_init();
  //PMC_ADDRESS.ESR_0.R = 0x193E0000; // Clear all flags in PMC_ESR_0 register
  *(volatile uint32_t *)0xFFFA0420 = 0x193E0000;//ESR
 
  *(volatile uint32_t *)0xFFFA0470 = 0x40000000;//FIR
 
  //PMC_ADDRESS.REE_0.R = 0x193E0000;
  *(volatile uint32_t *)0xFFFA0430 = 0x193E0000;//REE
 
  //PMC_ADDRESS.RES_0.R = 0x193E0000;
  *(volatile uint32_t *)0xFFFA0440 = 0x193E0000;//RES
 
  // Clear any previous fault flags to start fresh
  //MC_RGM->FES = 0xffffffff; // Clear all detected faults (write-1-to-clear)
 
  // Enable functional reset for specific fault
  //MC_RGM->FERD &= ~(1 << 7); // Enable reset for VOR faults
  //MC_RGM->FERD &= ~(1 << 28);     // Enable reset for software fault
 
  // Set fault action to RESET
  //MC_RGM->FEAR |= (1 << 7); // Action: Reset for VOR
  //MC_RGM->FEAR |= (1 << 28);     // Action: Reset for software fault
 
  //PMC_injectFakeFault(PMC_HVD_FAULT);
 
  //MC_RGM->DES |= (1 << 7);
  //MC_RGM->DES |= (1 << 28);
 
  //MC_ME ->MCTL = 0x00005AF0;
  //MC_ME ->MCTL = 0x0000A50F;
 
  while(1)
  {
      /* Insert a small delay to make the blinking visible */
      delay(720000);
      /* Toggle output value LED1 */
      PINS_DRV_TogglePins(PORT, (1<<LED));
  //PINS_DRV_ClearPins(PORT, (1<<LED)); // Led ON
 
      //PINS_DRV_SetPins(PORT, (1<<LED));
 
      //PINS_DRV_ClearPins(PORT, (1<<LED));
  }
 
what is the problem?
 
for the addresses, check below images:
ismaelwael_1-1732009714601.png
ismaelwael_2-1732009752954.png

 

 
And if you have a working example of PMC, i will be thankful to you.
 
regards.
 
0 项奖励
回复
1 回复

1,054 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Actually I have created example for PMC BIST,

https://community.nxp.com/docs/DOC-334416

and VD single test:

https://community.nxp.com/docs/DOC-334417

also the application note:

https://www.nxp.com/docs/en/application-note/AN12171.pdf

Please have a look.

Best regards,

Peter

 

0 项奖励
回复