MPC5744P, LinFlexD in UART mode affecting Hall sensor capture interrupts

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P, LinFlexD in UART mode affecting Hall sensor capture interrupts

2,537件の閲覧回数
peacethanima27
Contributor II

Hi

I am facing an issue with the BLDC motor commutation speed when LINFlexD communication is in progress. When I send the measured speed information to PC terminal using LINFlexD in UART mode, I find that the motor commutation is affected. Thinking this is due to the interrupt priorities, I have set the Hall sensor capture interrupt priority to a high value.

INTC_0.PSR[611].R = 0x801D;  //Set priority for external eTimer interrupt.

I am using the below example code for transmitting the values using LINFlexD

/*******************************************************************************
Function Name : TransmitData
Parameters : pBuf - input string. won't be modified by the function
: cnt - input number of characters to be transmitted
Notes : Tx data on LINFlexD_1. polled mode.
*******************************************************************************/
void TransmitData(const char *pBuf, uint32_t cnt)
{
uint8_t j = 0; // Dummy variable

for (j=0; j< cnt; j++)
{ // Loop for character string
LINFlexD_1.BDRL.B.DATA0 = *(pBuf+j);
//write character to transmit buffer
while (1 != LINFlexD_1.UARTSR.B.DTFTFF) {}
// Wait for data transmission completed flag
LINFlexD_1.UARTSR.R = 0x0002;
// clear the DTF flag and not the other flags
}
}

Can anyone help please?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,387件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if the TransmitData() is not called within other interrupt then there should not be an issue. If yes, then check if nested interrupts are enabled. With interrupt nesting allowed the interrupt handler contains necessary prolog and epilog and interrupts are enabled again during prolog allowing interrupt with higher priority to be called immediately.

So check your IVOR4 handler.

BR, Petr

 

0 件の賞賛
返信

2,387件の閲覧回数
peacethanima27
Contributor II

TransmitData() is called in a while loop at a scheduled interval (500msec), and not in a nested interrupt. That is why I was wondering how my commutation is affected. 

0 件の賞賛
返信

2,387件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

I can only recommend to check priorities of all enabled interrupts and be sure nested interrupts are allowed.

A normal interruptible code, TransmitData() you have, cannot affect interrupt generation.

BR, Petr

0 件の賞賛
返信