MPC5744P CTU ERRCMP error flag

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P CTU ERRCMP error flag

5,448件の閲覧回数
maitesierra
Contributor II

Hi,

 

We are working with MPC5744P and we have got an error flag (ERRCMP flag in CTU_EFR register) which appears as soon as we initialize CTU. The configured trigger signal for the CTU is I1_RE which corresponds  with FlexPWM0 submodule 0  VAL0. If we change TGSCCR register to 4801 or less value (< FlexPWM_0.SUB[0].VAL1), ERRCMP error flag is set when CTU is initialized and once per PWM cycle. But  if we change TGSCCR value to 5000 (or > FlexPWM_0.SUB[0].VAL1) ERRCMP error flag is set just when CTU is initiated.

 

Is there any way of avoiding this error first time CTU is initalized?

 

In Main program, we initialize CTU first and then we initialize FlexPWM as you can see in included functions at the end of the message.

 

Thanks in advance for your help.

Maite

 

void CTU_Init(void)

{

CTU_0.TGSISR.R = 0x00000004; // I1_RE (Input1: FlexPWM0 SubMod0 VAL0 VAL2 VAL4

CTU_0.THCR1.R = 0x00000061; //Enable Triger 0 and set to ADC

CTU_0.TCR[0].R = 1; // For triggering single conversion on ADC0

 

CTU_0.TGSCCR.R = 5000; // end value

CTU_0.TGSCRR.R = 0; // initial value

 

CTU_0.TGSCR.R = 0x0100; // Toggle mode for external trigger

 

//===== Set ADC messages 2 CHANNELS=====

CTU_0.FTH.R = 0x00000001; // set FIFO 0 threshold to 1, overflow is set when 2 results comes Max 8 bits

 

CTU_0.CLR[0].A.R = 0x4000; // Command 0 - first command in command sequence, sample ADC1-CH0, result to FIFO0

CTU_0.CLR[1].A.R = 0x0001; // Command 1 - next command in command sequence,sample ADC1-CH1, result to FIFO0

CTU_0.CLR[2].A.R = 0x4000; // stop the sequence, first command of second sequence which is not started

 CTU_0.CLR[0].A.B.SU = 1; // ADC_1 ch0

CTU_0.CLR[1].A.B.SU = 1; // ADC_1 ch1

 

CTU_0.FCR.R = 0x00000004; // FIFO 0 threshold overflow interrupt enable

 

CTU_0.CR.R = 0x0003; // General reload and TGS input selection reload

 

if(CTU_0.EFR.B.ERRCMP == 1)

  {

  CTU_0.EFR.B.ERRCMP = 1;

  SIUL2.GPDO[LED1].R = ~SIUL2.GPDO[LED1].R;

 }

}

 

void FlexPWM_Init(void)

{

 FlexPWM_0.OUTEN.R = 0x110;

//-----  control register ---

FlexPWM_0.SUB[0].CTRL1.R = 0x0400;

FlexPWM_0.SUB[0].CTRL2.R = 0x0000;

FlexPWM_0.SUB[0].TCTRL.R = 0x0001; // VAL0 reg determine OUT_TRIG0 generation

 

//----- INIT, VAL0, VAL1, VAL2, VAL3 -----

FlexPWM_0.SUB[0].INIT.R = 0; // init value

FlexPWM_0.SUB[0].VAL1.R = 4802; // end value

FlexPWM_0.SUB[0].VAL2.R = 0; // PWM A0 rising edge

FlexPWM_0.SUB[0].VAL3.R = 800; // PWM A0 falling edge

FlexPWM_0.SUB[0].VAL0.R = 0;

 

//-----  interrupt enable register ---

FlexPWM_0.SUB[0].INTEN.R = 0x1000; //reload

 

//========== LDOK (reload) & RUN (run PWMs) =========

FlexPWM_0.MCTRL.B.LDOK = 0x1; //submodule 0

FlexPWM_0.MCTRL.B.RUN = 0x1; // Submodule 0 PWM0 generator enabled

}

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

4,610件の閲覧回数
maitesierra
Contributor II

Hi Petr,

Thanks for your answer. We are working with reference manual Rev 5 which do not include this paragraph. Could you include Rev 6 pdf from the reference manual in this post please? As it is imposible to get it from web (web link is not working well as it goes to Rev 5 from reference manual)

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/32-bit-power-archite...

Many thanks,

Maite

0 件の賞賛
返信

4,607件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

see attached...

the link will be fixed.

BR, Petr

4,607件の閲覧回数
maitesierra
Contributor II

Thanks!!

Regards,

Maite

0 件の賞賛
返信

4,607件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi Maite,

This flag is set each time the CTU becomes clocked. See this info from the RM

 pastedImage_1.png

So just clear this flag during initialization.

BR, Petr

0 件の賞賛
返信