MPC5744 Transfer Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744 Transfer Error

Jump to solution
1,780 Views
Jamber_H
Contributor III

In the reference manual of 5744, there are many "transfer errors" case, such as write a protected register while Hard Lock Bit is set, or access an unimplemented registers, but what "transfer errors" mean? to assert an exception or assert a flag, or other response?

 

0 Kudos
Reply
1 Solution
1,771 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

transfer error is known also as bus error. It occurs when given address is not accessible for read or write. The access is terminated on internal bus and Machine Check (IVOR1) is triggered in this case. Take a look at section "5.7.2 Machine Check Interrupt (IVOR1)" where it is described in detail:

https://www.nxp.com/webapp/Download?colCode=E200Z4RM&location=null

The most important table is this one:

lukaszadrapa_0-1615194023652.png

 

Regards,

Lukas

 

View solution in original post

0 Kudos
Reply
1 Reply
1,772 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

transfer error is known also as bus error. It occurs when given address is not accessible for read or write. The access is terminated on internal bus and Machine Check (IVOR1) is triggered in this case. Take a look at section "5.7.2 Machine Check Interrupt (IVOR1)" where it is described in detail:

https://www.nxp.com/webapp/Download?colCode=E200Z4RM&location=null

The most important table is this one:

lukaszadrapa_0-1615194023652.png

 

Regards,

Lukas

 

0 Kudos
Reply