MPC5744 SENT driver compilation failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744 SENT driver compilation failed

Jump to solution
4,165 Views
gsr007
Contributor I

 Dear expert:  

    At S32DS,I tried  to run the SENT driver in AN4856 for 5744. But there are many compilation errors.

gsr007_1-1694488220470.pnggsr007_1-1694488220470.pnggsr007_2-1694488245137.pnggsr007_2-1694488245137.pnggsr007_3-1694488256740.pnggsr007_3-1694488256740.pnggsr007_4-1694488265180.pnggsr007_4-1694488265180.png

So,my questions include these points:

1.what is the root cause of the above problems? Are there errors in my project configuration?But I have run other drivers successfully before,for example the ADC driver,the CAN driver and so on.

2.How to solve these problems?

Also, I saw that someone had asked a similar question, but it was not resolved in the end.

Thanks.

 
0 Kudos
Reply
1 Solution
4,139 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

that driver/example was done in GreenHills so importing to teh S32DS could not be such easy and you need to do it yourself.
Anyway, there is SDK demo example for SENT receiver within S32DS, so you can refer to it;
c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5744P\driver_examples\communication\srx_fast_dma\Doxygen\srx_fast_dma_mpc5744p.dox

BR, Petr

View solution in original post

0 Kudos
Reply
4 Replies
4,140 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

that driver/example was done in GreenHills so importing to teh S32DS could not be such easy and you need to do it yourself.
Anyway, there is SDK demo example for SENT receiver within S32DS, so you can refer to it;
c:\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\examples\MPC5744P\driver_examples\communication\srx_fast_dma\Doxygen\srx_fast_dma_mpc5744p.dox

BR, Petr

0 Kudos
Reply
4,097 Views
gsr007
Contributor I

Thank you for your reply!

Also, I would like to know where to obtain this document?

Thanks!

0 Kudos
Reply
4,069 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it is just very short description of the demo example. So install SDK and you can locate it there.

BR, Petr

0 Kudos
Reply
4,067 Views
gsr007
Contributor I

Your replies are ver helpful to me.

Thank you very much.

0 Kudos
Reply