MPC5744 Clock Config problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744 Clock Config problem

3,115件の閲覧回数
shidongxing
Contributor I

Hi NXP Team:

I have the following problem configuring Clock:

I configured the clock source as IRC,when the XOSC is connected, the system goes well.

But if I removed XOSC from 5744, the program stuck at "getPllStatus"

here is my code:

void clk_init_IRC(void)
{
SysClk_Init();
InitPeriClkGen();
}

// Enable XOSC, PLL0, PLL1 and enter RUN0 with PLL0 as sys clk (100 MHz)
void SysClk_Init(void)
    {
     MC_CGM.AC3_SC.B.SELCTL = 0x00;         //connect IRC to the PLL0 input
     MC_CGM.AC4_SC.B.SELCTL = 0x03;         //connect PLL0-PHI1 to the PLL1 input
    
     // Set PLL0 to 100 MHz with 16MHz IRC reference
     PLLDIG.PLL0DV.R = 0x30041019;  // PREDIV = 1, MFD = 25, RFDPHI = 4, RFDPHI1 = 6
    
     MC_ME.RUN0_MC.R = 0x00130070;      // RUN0 cfg: IRCON,OSC0ON,PLL0ON,syclk=IRC
    
     // Mode Transition to enter RUN0 mode:
     MC_ME.MCTL.R = 0x40005AF0;         // Enter RUN0 Mode & Key
     MC_ME.MCTL.R = 0x4000A50F;         // Enter RUN0 Mode & Inverted Key
     while (MC_ME.GS.B.S_MTRANS) {};        // Wait for mode transition to complete
     while(MC_ME.GS.B.S_CURRENT_MODE != 4) {};  // Verify RUN0 is the current mode
    
     // Set PLL1 to 200 MHz with 66.6666666666667MHz PLL0-PHI1 reference
     PLLDIG.PLL1DV.R = 0x00030012;  // MFD = 18, RFDPHI = 3
    
     MC_ME.RUN_PC[0].R = 0x000000FE;        // enable peripherals run in all modes
     MC_ME.RUN0_MC.R = 0x001300F2;      // RUN0 cfg: IRCON, OSC0ON, PLL1ON, syclk=PLL0
    
     MC_CGM.SC_DC0.R = 0x80030000; // PBRIDGE0/PBRIDGE1_CLK at syst clk div by 4 ... (25 MHz)
    
     // Mode Transition to enter RUN0 mode:
     MC_ME.MCTL.R = 0x40005AF0;         // Enter RUN0 Mode & Key
     MC_ME.MCTL.R = 0x4000A50F;         // Enter RUN0 Mode & Inverted Key
     while (MC_ME.GS.B.S_MTRANS) {};        // Wait for mode transition to complete
     while(MC_ME.GS.B.S_CURRENT_MODE != 4) {};  // Verify RUN0 is the current mode
}
void InitPeriClkGen(void)
{
     // MC_CGM.SC_DC0.R = 0x80030000; // PBRIDGE0/PBRIDGE1_CLK at syst clk div by 4 ... (25 MHz)
     MC_CGM.AC0_SC.R = 0x02000000; // Select PLL0 for auxiliary clock 0
     MC_CGM.AC0_DC0.R = 0x80000000; // MOTC_CLK : Enable aux clk 0 div by 1 … (100 MHz)
     MC_CGM.AC0_DC1.R = 0x80070000; // SGEN_CLK : Enable aux clk 0 div by 8 … (12.5 MHz)
     MC_CGM.AC0_DC2.R = 0x80010000; // ADC_CLK : Enable aux clk 0 div by 2 … (50 MHz)
     MC_CGM.AC6_SC.R = 0x02000000; // Select PLL0 for auxiliary clock 6
     MC_CGM.AC6_DC0.R = 0x80010000; // CLKOUT0 : Enable aux clk 6 div by 2 … (50 MHz)
     MC_CGM.AC10_SC.R = 0x02000000; // Select PLL0 for auxiliary clock 10
     MC_CGM.AC10_DC0.R = 0x80030000; // ENET_CLK : Enable aux clk 10 div by 4 … (25 MHz)
     MC_CGM.AC11_SC.R = 0x02000000; // Select PLL0 for auxiliary clock 11
     MC_CGM.AC11_DC0.R = 0x80030000; // ENET_TIME_CLK : Enable aux clk 11 div by 4 … (25 MHz)
     MC_CGM.AC5_SC.R = 0x02000000; // Select PLL0 for auxiliary clock 5
     MC_CGM.AC5_DC0.R = 0x80000000; // LFAST_CLK : Enable aux clk 5 div by 1 … (100 MHz)
     MC_CGM.AC2_DC0.R = 0x80010000; // CAN_PLL_CLK : Enable aux clk 2 (PLL0) div by 2 … (50 MHz)
     MC_CGM.AC1_DC0.R = 0x80010000; // FRAY_PLL_CLK : Enable aux clk 1 (PLL0) div by 2 … (50 MHz)
     MC_CGM.AC1_DC1.R = 0x80010000; // SENT_CLK : Enable aux clk 1 (PLL0) div by 2 … (50 MHz)
}
the program stuck at:
while (Mcu_GetPllStatus() != MCU_PLL_LOCKED)
{
}
after function call :clk_init_IRC
why would this happen? Did I miss anything?
Thanks!
ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,847件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

When you have active peripherals running from PLL sourced by XOSC, you have to first change the clocks in CGM module to IRC for those peripherals and then you can disable XOSC.

regards,

Peter

0 件の賞賛
返信

2,847件の閲覧回数
erreer
Contributor I

Hi,When we have active peripherals running from PLL sourced by XOSC, we have to first change the clocks in CGM module to IRC for those peripherals and then we can disable XOSC, what about the active  peripherals is ?

for example :

MC_ME.RUN_PC[0].B.DRUN=0;//

But I don't use CAN and PIT  peripheral, howerer ,the CAN and PIT clock is  XOSC and  SYSCLK CLOCK default , if i want  switch mode, what should i do ?

0 件の賞賛
返信