MPC5676R Internal Temperature Sensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5676R Internal Temperature Sensor

1,358件の閲覧回数
nicklabianco
Contributor I

The datasheet for this device states that the accuracy is +/- 10 degrees Celsius. Is this true if the internal calibration constants are used or can you obtain a better accuracy when using the internal calibration parameters?

ラベル(1)
0 件の賞賛
返信
1 返信

1,280件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

These internal sensors are typically quite imprecise, thus +/-10 °C is valid even it is calibrated in accordance to reference manual. Of course accuracy will be better than +/-10 °C as these values are corner cases.

0 件の賞賛
返信