MPC5676R Internal Temperature Sensor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5676R Internal Temperature Sensor

1,351 次查看
nicklabianco
Contributor I

The datasheet for this device states that the accuracy is +/- 10 degrees Celsius. Is this true if the internal calibration constants are used or can you obtain a better accuracy when using the internal calibration parameters?

标签 (1)
0 项奖励
回复
1 回复

1,273 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

These internal sensors are typically quite imprecise, thus +/-10 °C is valid even it is calibrated in accordance to reference manual. Of course accuracy will be better than +/-10 °C as these values are corner cases.

0 项奖励
回复