MPC5676R, ADC trigger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5676R, ADC trigger

1,565 Views
jangpr
Contributor I

I am using the MPC5676R. Currently, ADC trigger is used for motor control by using fs_etpu_asac_init. In addition to this trigger point, I want to use one more internal software trigger to sense some values before existing trigger point. I used the ASAC function once again, but the code stopped during the code initialization. 

1) I want to know how to use multiple software triggers.

2) I want to know if there is a related sample file.

eQADC‌ , ASAC , 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,477 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am not sure if this question is related to eTPU or not.

In principle eQADC commands are executed according priorities of command queues. Pay attention to following thread, the picture in the middle of the communication

MPC5777C EQADC configuration  

Hope it helps

0 Kudos
Reply