MPC5674F series micro controller output levels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5674F series micro controller output levels

875 次查看
prachi_moghe
Contributor I

Hi, 

I am using NXP MPC5674F series microcontroller (Part number: SPC5674FF3MVY3) in the design.

I have  a query for output voltage levels for this part.

For V.DDEH supply of 5V, V.OH_S and V.OL_S levels are mentioned considering I.OH_S= 11.6mA and I.OL_S= 17.7mA respectively. (Datasheet Rev. 10.1, 06/2015).

Could you please provide these voltage values for current 1mA or less.

 

Also please consider following method that I am following.

With Vcc=5V

  1. For low level output voltage level (V.ol)

V.OL= 0.2*Vcc = 1V for I.OL= 17.7 mA (from datasheet)

R.OL= V.OL/I.OL= 56.49 Ohm

With R.OL= 56.49 Ohm and current less than or equal to 1mA,

V.OL_1mA= R.OL*1mA= 56.49 mV

 For high level output voltage level (V.oh)

V.OH= 0.8*Vcc = 4V for I.OH= 11.6mA (from datasheet)

R.OH= (Vcc- V.OH)/ I.OH= 86.2 Ohm

With R.OH= 86.2 Ohm and current less than or equal to 1mA,

V.OH_1mA= Vcc - (R.OH* 1mA)= 4.9138 V

Please confirm if this understanding is correct.

0 项奖励
回复
1 回复

802 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, this characteristic can be linearly extrapolated, so your calculation is correct.

Regards,

Lukas

0 项奖励
回复