MPC5674F EMIOS CBDR Value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5674F EMIOS CBDR Value

跳至解决方案
2,252 次查看
erdincnamal
Contributor II

Hi,

I tried to assign "0" decimal value to EMIOS' CBDR register. After I set the value to 0 (without resetting), in my next duty-frequency change attempts, when I tried a value that would give 50% duty (CADR = 500, CBDR = 1000), I saw that I could not produce PWM. This problem continued until I reset it. 

My question is, do I need to do such a range check and is the reference available in the manual or in a different document? Unfortunately, most links related to EMIOS in the forum are broken. I would be happy if you help.

Best regards,

Erdinc

标记 (3)
0 项奖励
回复
1 解答
2,227 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi

you did not mention mode used. So refer to chapter 22.4.1.1 Unified Channel Modes of Operation of the device Reference Manual for mode description and explanation for CARD/CBDR register values and usage for each modes. 

BR, Petr

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,222 次查看
erdincnamal
Contributor II

Thanks I found

0 项奖励
回复
2,228 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi

you did not mention mode used. So refer to chapter 22.4.1.1 Unified Channel Modes of Operation of the device Reference Manual for mode description and explanation for CARD/CBDR register values and usage for each modes. 

BR, Petr

0 项奖励
回复
2,225 次查看
erdincnamal
Contributor II
I use in mode 101_1010 OPWFMB Output Pulse Width and Frequency Modulation Buffered, (flag on A or B matches)
0 项奖励
回复