MPC5646c flexray

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,885件の閲覧回数
boyoungmun
Contributor I

Hi

 

I wonder whether MPC5646c(motherboard XPC56xx) supports 2 flexray channels(A and B) or not.

In XPC56xx user manual, I can see the 2 flexray transceivers are connected a same DB9M connector. 

It means that both flexray channels are available?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,734件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

pastedImage_1.png

So, both channels are supported but it is necessary to solder second transceiver on the board.

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,735件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

pastedImage_1.png

So, both channels are supported but it is necessary to solder second transceiver on the board.

Regards,

Lukas

0 件の賞賛
返信
2,734件の閲覧回数
boyoungmun
Contributor I

Dear Lukas,

 

In XPC564B user manual, the board already have two FlexRay transceivers. Is an additional transceiver needed?

0 件の賞賛
返信
2,734件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

There's sentence: "However, only one circuit is assembled by default."

You can see that here:

pastedImage_1.png

Regards,

Lukas