MPC5644A : flash memory problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5644A : flash memory problem

1,213件の閲覧回数
gianlucadall_ag
Contributor I

Hi

I implemented a bootloader code on MPC5644A, this code erases the flash memory and after that programs s-record file sent via CAN.

Even if the bootloader code works well and  the application code ether,

(the bootloader start address is 0x40000 and the application code start address is 0xC0000)

when the code jump to application code start address, something goes wrong


below attached the error message

 

IVOR1trap:  bIVOR1trap // Machine check / (NMI) interrupt handler

                             // ISI, ITLB Error on first instruction fetch for an exception handler

                             // Parity Error signaled on cache access

                             // External bus error

 

what kind of problem could be this?

could anyone help me?


thanks


Gianluca

ラベル(1)
0 件の賞賛
返信
0 返答(返信)