MPC5644A eQADC ch 128 not returning valid temperature sensor value

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5644A eQADC ch 128 not returning valid temperature sensor value

3,368 次查看
williamtroyjr
Contributor I

I am trying to get the MCU temperature on an

 

SPC564A70L7

 


TTSENS_CODE(TLOW) is 0x1647(-40C)

TTSENS_CODE(THIGH) is 0x1D61(150C)

VBG_CODE(TLOW) is 0xF7F

Temperature sensor is ch 128 and returns values roughly 0x16A0 at room temperature/normal running.

Bandgap is ch 45 and returns values roughly 0x1000.


When temperature formula is applied (MPC5644ARM pp 1231), (TTSENS_CODE(T) X B) calculates to a value less than TTSENS_CODE(TLOW) which should be impossible. The reading from ch 128 when bandgap adjusted is below the -40C value. What is wrong?


eQADC is calibrated and works just fine reading various internal voltage and the bandgap.

 


标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

3,053 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

If the TTSENS_CODE(T) X B gives you value below TTSENS_CODE(TLOW), then the calculated temperature must be below TLOW. This can happen, I think. Take into account the TSENS accuracy, also the ADC accuracy itself.

Hard to say, Are you sure the TLOW is -40?

I have upload the MPC5644A TSENS calculation example on https://community.freescale.com/docs/DOC-104692. 

Try to use it.

Regards,

Petr

0 项奖励
回复

3,045 次查看
williamtroyjr
Contributor I

Hello,

I reviewed the sample and verified that the formula I implemented is working correctly.

TSENS_CODE(T)B can be reduced to VTSENS(T)VBG_CODE(TLOW)/VBG_CODE(T) thereby eliminating the need to sample for VREF.

The problem is the TSENSE low constant stored at FFFEC000. I get a value which appears incorrect. The high constant and bandgap values appear correct.

My values:

FFFEC000(TSENS_TCCR0) -> $DD615627 which corresponds to: 150C with TSENS_CODE(THIGH) of $1D61 and -40C with TSENS_CODE(TLOW) of $1627.

FFFEC004(TSENS_TCCR1) -> $0F7FXXXX which is $F7F for VBG_CODE(TLOW)

Your values:

FFFEC000(TSENS_TCCR0) -> $9C891541 which corresponds to: 145C with TSENS_CODE(THIGH) of $1C89 and 25C with TSENS_CODE(TLOW) of $1541.

FFFEC004(TSENS_TCCR1) -> $0FAAXXXX which is $FAA for VBG_CODE(TLOW)

The value you read for TLOW is $1541 for 25C. I read $1627 for -40C. This is impossible! The lower the temperature, the lower the voltage not higher. I believe the value you are reading is correct. The value I am reading is clearly wrong. Where there chips with incorrect TLOW temperature constant manufactured for STM?

I am using a discovery board made by STMicro called SPC564A-DISC containing an SPC564A70L7 chip. The specs on the chip are 150Mhz, 150C to -40C, 1.5MB Flash and 128KB SRAM. Otherwise it is the same as a MPC5644A. Freescale’s and STM’s reference manuals are equivalent for the eQADC and temperature sensor sections.

We are in the process of producing the first 5 vehicle controllers using an SPC5644AMLU1 chip. I hope that chip contains correct TSENSE constants. I will adjust my code to handle the faulty SPC564A70L7 chip.

For now, my query has been answered

Thanks,

William A Troy Jr

DHTE

0 项奖励
回复