MPC5644A VDDREG operating range?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5644A VDDREG operating range?

ソリューションへジャンプ
3,284件の閲覧回数
cthhk
NXP Employee
NXP Employee

Dear Support:

 

According to datasheet, VDDREG should be within 4.75~5.25V. The question is, what happens if it falls to lower than 4.75V?

We are using internal 3.3V regulator and internal 1.2V regulator so we need to make sure if they still work normally till LVD happens.

 

Your quick response would be highly appreciated!

 

Best Regards,

WY

ラベル(1)
0 件の賞賛
返信
1 解決策
3,131件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

AN4291, chapter 3.1.1 says:

“If VDDREG is less than 4.5 V, then the 3.3 V regulator is disabled”

There will some safety margin, but in my opinion disabling of 3.3 V regulator can happen is VDDREG it falls to lower than 4.75V.

http://cache.nxp.com/files/32bit/doc/app_note/AN4291.pdf

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,132件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

AN4291, chapter 3.1.1 says:

“If VDDREG is less than 4.5 V, then the 3.3 V regulator is disabled”

There will some safety margin, but in my opinion disabling of 3.3 V regulator can happen is VDDREG it falls to lower than 4.75V.

http://cache.nxp.com/files/32bit/doc/app_note/AN4291.pdf

0 件の賞賛
返信
3,131件の閲覧回数
cthhk
NXP Employee
NXP Employee

hi David:

I need to append one more question: If we use 5V for all GPIO, 3.3V is only connected to NEXUS module. Then can we say 3.3V can be ignored and won't affect anything else in normal mode?

I'm asking this because we need to design the external reset circuit to guarantee that the whole system is always working before reset asserted... If 3.3V could be ignored in such case, the external circuit will be much simpler.

Best Regards,

WY.

0 件の賞賛
返信
3,131件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Even though VDDEH7 voltage is being powered by 5V, when nexus functionality for nexus pads is selected, these pads will have 3.3V level (MultiV output in low-swing mode).

So yes, you can build 5V only system (considering core voltage powered by internal regulator).

0 件の賞賛
返信
3,131件の閲覧回数
cthhk
NXP Employee
NXP Employee

hi David:

Clear and thank you very much!

Best Regards,

WY

0 件の賞賛
返信