MPC5643L Flash Driver Support Need

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5643L Flash Driver Support Need

1,207件の閲覧回数
DanielDuJijun
Contributor III

Dear NXP Support Team.

There are a few questions I would like to ask about flash:
1. Whether it is necessary to initialize when using on-chip Flash of MPC5643L?
2. The programme flow provided in the chip manual, but it will not be able to write.

3.I followed the erase procedure in the chip's manual, and it doesn't erase it either.

4.Please help to Provide a flash driver demo project that can be programmed/erased properly?
5. Part of the sample code is as follows:

タグ(1)
0 件の賞賛
返信
1 返信

1,166件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I suppose you mean runtime programming. It is easiest to use SSD driver, I would recommend to use. On the product webpage you may find in section ‘Software’ and file is called ‘MPC56xx C90FL JDP Standard Software Driver for Single-Module Flash’

https://www.nxp.com/products/processors-and-microcontrollers/power-architecture/mpc5xxx-microcontrol...

 

Also I could point out following example showing simple programming without using of SSD drivers:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5643L-Flash-program-simple-CW210/ta-p...

0 件の賞賛
返信