MPC5643L Boot without VDD_HV_ADR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5643L Boot without VDD_HV_ADR

1,256 次查看
jinjingyang
NXP Employee
NXP Employee

Dear Sir,

 

I tested on MPC5643L EVB and found that the MCU can boot without applying VDD_HV_ADR.

But it get stuck at the following code:

//ME_GS Wait for external osc to stabilize.

    while(ME.GS.B.S_XOSC==0)    {};

Even I applied 5V to VDD_HV_ADR at this moment, the software was still stuck here.

Then I reset the MCU and it can run normally and complete all clock initialization.

 

Can you help explain the above boot process? Why would I be stuck at the crystal initialization?

And customer's question is what's the max allowed delay between VDD_HV_ADR and other supplies for MCU to boot successfully at the very first time.

 

Regards,

Jason Yang

标签 (1)
0 项奖励
回复
1 回复

1,183 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Jason,

I think that this note from datasheet explains everything:

pastedImage_1.png

Regards,

Lukas

0 项奖励
回复