MPC5634M Power Pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5634M Power Pins

1,876 Views
rayhall
Contributor V

Hello,

 

Is there a application note or schematic, that shows recommended power pins/pads circuit for the MPC5634M

 

I am using the 208 BGA version.

 

Ray.

Labels (1)
0 Kudos
Reply
3 Replies

1,732 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Unfortunately we do not have a specific hardware design guide for the MPC5634M device. I could recommend you some general or MPC55xx appnotes that could be useful:

AN3254 - Power Supplies on the MPC5500:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3254.pdf

AN3208 - Crystal Oscillator Troubleshooting Guide:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN3208.pdf

AN1706 - Microcontroller Oscillator Circuit Design Considerations:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN1706.pdf

AN1259 - System Design and Layout Techniques for Noise Reduction:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN1259.pdf

AN2706 - EMC Guidelines for MPC5500-Based Systems:

http://www.nxp.com/files/32bit/doc/app_note/AN2706.pdf

AN2705 - Signal Integrity Considerations with MPC5500-based systems:

http://www.nxp.com/files/32bit/doc/app_note/AN2705.pdf

AN2127 - EMC Guidelines for MPC Based Automotive Powertrain Systems:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN2127.pdf

Also there is a document for MPC5644A that is similar device:

http://www.nxp.com/files/32bit/doc/app_note/AN4291.pdf

I would recommend you to follow up our EVB board that can be considered as reference design:

http://www.nxp.com/webapp/sps/site/prod_summary.jsp?code=XPC563MKIT&fr=gtl

http://www.nxp.com/webapp/sps/site/prod_summary.jsp?code=TRK-MPC5634M&fsrch=1

0 Kudos
Reply

1,732 Views
rayhall
Contributor V

David,

Thank you for the links. In all the documentation I have read, shows the VDD pins being powered via a BCP68 that is controlled by the VRCCTL pin.

Can the VDD pins be powered directly by 5 volts, so the BCP68 circuit is not used.

I am thinking the BCP68 circuit is so the micro can use less energy. I have a 110 amp alternator as the power supply and this is driven by a 500 hp engine. I am not really struggling for electrical energy/power.

Ray.

0 Kudos
Reply

1,732 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, it cannot be powered directly by 5V.

VDD is 1.2V voltage domain, it must be powered by 1.2V+-10%, the voltage is allowed to be powered externally (i.e. without bypass transistor), in this case voltage range is even tighter (1.26V-1.32V).

0 Kudos
Reply