MPC5606S Minimum PowerUp Requirements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5606S Minimum PowerUp Requirements

1,398件の閲覧回数
Daniel-9876
Contributor I

Dear Ladies and Gentlemen, 

I need to exchange the MCU of an existing board, cause the original MCU is dieing the heat-death.

It is MPC5606SVLU

When I place the new MCU, I can see every powersupply is available on the MCU and the internal 1.2V regulator of the MCU is working well. 

My Oscillators, the main oscillator as well as the rtc oscillator, are not running, RESET is high. 

Depending on that, I am not able to flash it with JTAG. 

Is there a documentation of the minimum powerup requirements of this chip, so I can figure out what is going wrong? 

I wanted to try to programm it with XPC560SKIT176S, but this is not available for me now. 

Thank you in advance  

0 件の賞賛
返信
2 返答(返信)

1,347件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Crystal circuit should be as follows (AN4719), especially check VREG_BYPASS pin connection (it must not be floating.

davidtosenovjan_0-1637585251853.png

https://www.nxp.com/docs/en/application-note/AN4719.pdf

Also you could consult with EVB schematics.

 

 

0 件の賞賛
返信

1,349件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Power sequence you may see stated in the datasheet:

davidtosenovjan_0-1637584981310.png

davidtosenovjan_1-1637585021889.png

 

 

0 件の賞賛
返信