MPC5605B DFLASH issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5605B DFLASH issue

3,891件の閲覧回数
曾经怀念
Contributor II

Hi,

 

   pastedImage_1.png

  

From the data sheet, it seem i have to wait for 300~500ms when erase DFLASH.

What is the risk if i open the external interrupts after enable EHV , or non-blocking

0 件の賞賛
返信
6 返答(返信)

3,723件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it does not mean user would have to set up this wait time manually. After starting erase operation application polls MCR[DONE] bit.
However erase time may differ from piece-to-piece and it is also given by aging of flash memory.

0 件の賞賛
返信

3,723件の閲覧回数
曾经怀念
Contributor II

Hi David,

      

as usually:close external interrupts => EHV=1 => waiting for DONE => EHV=0 => open external interrupts;

change     :close external interrupts => EHV=1 => open external interrupts=> polls MCR[DONE] => EHV=0;

We need to assess the risk of change

0 件の賞賛
返信

3,723件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, there is a risk of read-while-write operation in case user software wants to read from the memory during erase/program. It would lead either in bus error or execution stall (according to RWWC, on this device stalls by default).

A solution is to have interrupt vector table and interrupt/exception service routine placed in SRAM.

0 件の賞賛
返信

3,723件の閲覧回数
malekben
Contributor II

Even if interrupt/exception service routine are placed in FLASH that would be in the CFlash not in teh DFlash ...

0 件の賞賛
返信

3,723件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you are right. I have somehow forgot we are talking about DFLASH. In case case it should be OK unless interrupt service routine does not access DFLASH.

0 件の賞賛
返信

3,723件の閲覧回数
曾经怀念
Contributor II

Hi David,

      in this p time need to pay attention to what?

     Is there a special document to introduce this?

Thanks!

0 件の賞賛
返信