MPC5604S - Flash library issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5604S - Flash library issue

1,583件の閲覧回数
akhilprasad
Contributor III
I am using MPC5604S controller and the self-programming flash library provided from NXP. I have a requirement to write certain numbers to a particular memory location using the flash write operation. But one constrain is that i need to refresh the controller in every 10ms else the controller will reset or go to sleep. So i am refreshing watchdog inside the callback routine. 
But the issue I am facing is that when I am trying to write the number to the controller using flash library,the controller is resetting. That means watchdog refreshing is not happening.
Kindly provide your suggestions ASAP.
0 件の賞賛
返信
1 返信

1,493件の閲覧回数
akhilprasad
Contributor III

Now this resetting issue is happening only when I am trying to write the number through CAN to the board and the board is stand alone i.e without connecting debugger.

0 件の賞賛
返信