MPC5604P for EPS and Quadrature Decoder Module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5604P for EPS and Quadrature Decoder Module

1,335 次查看
Hang_Yang_O
Contributor I

We are considering using MPC5604P as the microcontroller for EPS(Electric Power Steering). Now the developer requires Quadrature Decoder Module, while I looked through the user guide but it seems there isn't one. So my question is: is it possible to stick to the microcontroller/hardware to create the QE module? More generally, is a Module a set of Hardware(if w/o then not possible to use the functionalities) or the combination of common hardware with software on top of them?

Sorry for lack of knowledge for the topic. If the second question is confusing please just ignore it, I really need to find answer for the first one.

Thanks in advance.

0 项奖励
回复
1 回复

1,316 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

 

obviously eTimer channel in Quadrature count mode is used on this part.
See for example some motor control AN, like https://www.nxp.com/docs/en/application-note/AN4561.pdf

 

BR, Petr

0 项奖励
回复