MPC5604E - Viewing AVB videostream

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604E - Viewing AVB videostream

3,023 Views
thiesteichmann
Contributor II

Hello everyone,

i have another question. I've tried viewing the videostream with the VLCplayer, but it has a huge delay. So i tried viewing it with openCV, but the lower half of the video is stuttering (upper half is running smoothly). So i figured trying AVB would be a good idea. Does anyone know a way/tool to view the AVB videostream? Kuan Hung Lin can you help me with this, as you did with my problem last week?

Best regards

Thies

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

2,618 Views
kentlin
NXP Employee
NXP Employee

Hi Thies,

you can reduce the cashing of VLC player to have better reponse.

Capture1.JPG

I didn't try the AVB firmware either.

Best Regards,

Kent

0 Kudos
Reply

2,618 Views
thiesteichmann
Contributor II

Thanks, vlc works better this way. Additionally i now use Technica Engineering's Ethernet Video Analyzer software, which is capable of displaying the AVB videostream. Next problem is changing the ip address, which i will describe in the appropriate thread: MPC5604E - Data via BroadR-Reach

0 Kudos
Reply

2,618 Views
rsm911
Contributor I

Could you or someone supply the required *.sdp file contents for receiving H.264 over AVB stream and displaying in VLC ?   I have looked elsewhere on the web without success, even on the VLC website.   Thanks in advance.

0 Kudos
Reply