MPC5604E FEC & fNET

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5604E FEC & fNET

2,251 次查看
suhass
Contributor II

Hi,

I'm working on MPC5604E, using its Fast Ethernet Controller[FEC], & trying to initialize FNET stack on it, but according to "FNET Embedded TCP/IP Stack ", MPC5604E is not supported. [Refer the Image below]

 175080_175080.PNGfnet.PNG

Thanks & Regards

SUHAS S

标签 (1)
标记 (4)
0 项奖励
回复
2 回复数

2,034 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Suhas,

From my point of view FNET stack can be used with MPC5604E, but author does not support FNET for the listed platforms anymore as Patrice mentioned above.

Regards,

Martin

0 项奖励
回复

2,034 次查看
Pat
Contributor III

Dear Suhas,

I easily ported fNET on MPC5744P. The MCU dependent files are well identified/organized. Take a look on this thread FNET - Embedded TCP/IP Stack / FNET User Forum / FNET User Forum:Import FNET stack to MPC5748G 

Once the porting completed, you can add/share your files in the fNET. Of course the new one will not be supported even if there is no change. The author can't test fNET on all platforms.

Best regards,

Pat

0 项奖励
回复