MPC5604E Clock Architecture Issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5604E Clock Architecture Issues

1,719 次查看
suhass
Contributor II

Hi,

I'm working on MPC5604E, and wanted to get clock out of "clk_out" pin [PCR36, Pin No. 62], according to Clock Architecture Block diagram [Refer "Img1"], Input to the "clk_out" pad is from FMPLL_0 after FMPLL_CLK_DIV, But according to over experimentation its not the case, according to what I have validated the input to "clk_out" is from FMPLL_0 before FMPLL_CLK_DIV. It also says maximum frequency supported on "clk_out" pad is 32MHz [Refer Img2]

but we have tested it upto 120MHz. Do clarify the issues.

169441_169441.pngpastedImage_1.png

169445_169445.pngpastedImage_2.png

 

 

Thanks & Regards 

SUHAS S

标签 (1)
0 项奖励
回复
1 回复

1,602 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I have confirmed the same behavior on my board. Yes, the input for clk_out is before the divider. Thanks for pointing this out, I will report it.

Yes, it is possible that the clk out can be set to higher frequencies but we do not guarantee the functionality of the device in this case. It's out of our specification.

Regards,

Lukas

0 项奖励
回复