i want to know whether MPC5604 is support CAN3,the MPC5604B/C Microcontroller Data Sheet write that CAN0, CAN3 and either CAN1 or CAN4 are available. CAN2, CAN5 and CAN6 are not available,but the MPC5604B/C Microcontroller Reference Manual write that CAN0, CAN1 and CAN2 are available. CAN3, CAN4 and CAN5 are not available.
Hi,
as far as I know the RM's footnote 7 is wrong, the correct is the one from DS; CAN0, CAN3 and either CAN1 or CAN4 are available. CAN2, CAN5 and CAN6 are not available.
So except of 64pin MPC5604B, the CAN3 is available.
BR, Petr