MPC5566: what the input voltage range is for DATA30/ RXD2/GPIO58 pin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5566: what the input voltage range is for DATA30/ RXD2/GPIO58 pin?

993件の閲覧回数
shenmengting
Contributor I

My project  use MPC5566.And one digital input signal SW14 is used to monitor KEYSWITCH signal which is equal to vbattery(up to 32V).It's connected to DATA30 pin of MPC5566.My question is what the input voltage range is for this pin?

ラベル(1)
0 件の賞賛
返信
1 返信

940件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

See items 12/13 (VIH_F, VIL_F) of the device datasheet; http://cache.freescale.com/files/32bit/doc/data_sheet/MPC5566.pdf.

If input voltage is going to be higher then max specified you should use the serial resistor to limit the injection current (max 2mA).

Regards,

Petr

0 件の賞賛
返信