MPC5566: what the input voltage range is for DATA30/ RXD2/GPIO58 pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5566: what the input voltage range is for DATA30/ RXD2/GPIO58 pin?

1,007 次查看
shenmengting
Contributor I

My project  use MPC5566.And one digital input signal SW14 is used to monitor KEYSWITCH signal which is equal to vbattery(up to 32V).It's connected to DATA30 pin of MPC5566.My question is what the input voltage range is for this pin?

标签 (1)
0 项奖励
回复
1 回复

954 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

See items 12/13 (VIH_F, VIL_F) of the device datasheet; http://cache.freescale.com/files/32bit/doc/data_sheet/MPC5566.pdf.

If input voltage is going to be higher then max specified you should use the serial resistor to limit the injection current (max 2mA).

Regards,

Petr

0 项奖励
回复