MPC555LFAZP40 & MPC555LFMVR40

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC555LFAZP40 & MPC555LFMVR40

1,383件の閲覧回数
jmbrown
Contributor I

Hello,
What are the differences between MPC555LFAZP40 & MPC555LFMVR40?
What limitations exist in using the 2nd PN as a substitute for the 1st?
Thanks!
Jim Brown, [email protected]

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,371件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @jmbrown 

Ordering information can be found in this archived selector guide:

https://www.nxp.com/docs/en/product-selector-guide/SG1001.pdf

MPC5xx devices can be found on pages 4 and 5. Package designator description is missing on this page but you can check next page for MPC55xx devices, you can see that ‘ZP’ was used for SNPB version, ‘VR’ for PB-FREE version (these two versions were available).

In case of MPC555LFAZP40 & MPC555LFMVR40 - both devices contains the same silicon mask set 2K62N, so there are no functional differences. The difference is in temperature range and in SNPB / PB-FREE package.

Regards,
Lukas

0 件の賞賛
返信

1,341件の閲覧回数
jmbrown
Contributor I

Thank you Lucas, that was very helpful.

Jim

0 件の賞賛
返信