MPC555LFAZP40 & MPC555LFMVR40

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC555LFAZP40 & MPC555LFMVR40

1,328 次查看
jmbrown
Contributor I

Hello,
What are the differences between MPC555LFAZP40 & MPC555LFMVR40?
What limitations exist in using the 2nd PN as a substitute for the 1st?
Thanks!
Jim Brown, [email protected]

标记 (1)
0 项奖励
回复
2 回复数

1,316 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @jmbrown 

Ordering information can be found in this archived selector guide:

https://www.nxp.com/docs/en/product-selector-guide/SG1001.pdf

MPC5xx devices can be found on pages 4 and 5. Package designator description is missing on this page but you can check next page for MPC55xx devices, you can see that ‘ZP’ was used for SNPB version, ‘VR’ for PB-FREE version (these two versions were available).

In case of MPC555LFAZP40 & MPC555LFMVR40 - both devices contains the same silicon mask set 2K62N, so there are no functional differences. The difference is in temperature range and in SNPB / PB-FREE package.

Regards,
Lukas

0 项奖励
回复

1,286 次查看
jmbrown
Contributor I

Thank you Lucas, that was very helpful.

Jim

0 项奖励
回复