MPC5125 hang

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5125 hang

2,036件の閲覧回数
frank747
Contributor II

Hi all:

Mpc5125 doesn't start occasionally. We find the code hanging by lighting the indicator in. S and. C files.

It starts after the blr instruction of. S file and before the initialization PSC of. C file.
When the fault occurs, the poreset signal cannot restarts mpc5125. It must be powered off and then started. What is the possible reason.

The running process of the program is as follows.

in .s file
        ……
        ……
        mtlr r6
        mr r3, r2
        //led1               //run
        blr                   //hang start jump to .c file code

in .c file
        _WRS_ASM ("");
        vxSdaInit ();
        _WRS_ASM ("");
        pscInit();         //hang end
        //led2             //not run

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,031件の閲覧回数
Pavel
NXP Employee
NXP Employee

If this problem happens occasionally, this problem is not software problem.

Check your board using the Chapter 5 of the MPC5125 Datasheet:

https://www.nxp.com/docs/en/data-sheet/MPC5125.pdf

 

Often incorrect concerning to this chapter produces similar behavior.

0 件の賞賛
返信

2,025件の閲覧回数
frank747
Contributor II

Hi Pavel:

I found another problem on this board, The LPC_ CLK signal's frequency changes with temperature, and the relationship between frequency and temperature is similar to linear relationship. We use FPGA to collect LPC_CLK and counting,then lighting LED, we can find that the lighting frequency increases when the temperature decreases. When the temperature increases, the lighting frequency gradually decreases.

I checked my board using the Chapter 5 of the MPC5125 Datasheet. my board has some problems.

1.  some supplies reach the specified operating conditions after the PORESET be released. 

2. Unlike the recommended circuit, the PLL power supply uses magnetic beads instead of 10 ohm resistors.

Will these problems lead to the abnormality of my board? And  my board has started running, and then it hangs. Is this problem really irrelevant to the software?

0 件の賞賛
返信